DUG_Verhomoduuli ZB_WH-07

Shutter with tilting slats

  1. On the Home screen, tap .
  2. Tap Devices > Shutters > Shutter with tilting slats.
  3. Tap Open duration/Close duration (A) and enter the recorded shutter opening/closing time.
  4. Tap (B) and enter the slat tilt duration according to the tilt position.
    TÄRKEÄ: The minimum value to set the default time for Tilt duration is 01.00 s. If you set a value less than 01.00 s, it will not be saved.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Auttoiko tämä?