DUG_Water Leakage Sensor_WH-06

Using the device

The Control Panel of the Sensor allows you to monitor the current status of water leakage detection.
  1. On the Control tab, tap All devices or a room tab where the sensor is located

  2. On the Sensor control panel page, you can see the following:

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?