DUG_Water Leakage Sensor_WH-06

Checking the device history

Using the Wiser Home app, you can access the sensor history, which logs instances when water leakage was detected. Each event is recorded by the sensor and securely stored in the cloud.
NOTE: If the cloud connection is lost, the leakage detected events will not appear in the history.
  1. On the Control tab, tap All devices or a room tab where the sensor is located.
  2. On the device control panel page, tap History.
    TIP: The history page displays all logged-in events, even if the sensor notification toggle switch is disabled. For more information about sensor notification toggle switch, refer to Setting device notification.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?