DUG_Water Leakage Sensor_WH-06

Setting device notification

Using the Wiser Home app, you can enable or disable the sensor notification.
  1. On the Home screen, tap .
  2. Tap Devices > Water Leakage Sensor > Notify me if leak is detected (A) to enable or disable the sensor notification toggle switch.
    TIP: Additionally, you can enable or disable the sensor notification toggle switch by tapping on the Control tab, Water Leakage Sensor > Device settings > Notify me if leak is detected (A).
    NOTE:
    • Sensor notification toggle switch (A) is OFF by default.

    • Notifications created via automation are treated as separate notifications.

    • When the sensor detects water, it sends a notification and activates a sound alarm. The alarm will continue to sound until the sensor is removed from the water.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.