DUG_Wiser Connected Curtain Controller 2M-00

About the device

The Connected Curtain Controller (hereinafter referred to as module) is used to open and close blinds via switches. The module can be operated manually or through the Wiser app.

Devices controlled using curtain controller:

  • Curtains

  • Blinds

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.