DUG_Wiser Connected Curtain Controller 2M-00

Opening/Closing the curtain using app

Using the Wiser app, you can open/close the curtain.

To open/close:

  1. On the Home screen, tap Devices > Devices.
  2. Tap the shutter controller device.
    The Device Control Screen appears.
  3. Tap the following options to control the curtain:
    • Open (A): Tap to open the shutter.

    • Stop (B): Tap to stop the curtain at any position when it is opening/closing.

    • Close (C): Tap to close the shutter.

    • Shutter Percentage (D): Drag the bar to set the percentage of how much the shutter opens.

    TIP: You can also select the shutter controller device to open/close when you add it to your Favourites. To know more about Favourites, refer to the Add Favourites topic.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.