DUG_Wiser Connected Curtain Controller 2M-00

LED indication

Pairing

User Action

LED Indication

Status

Press the push-button 4 times in 10 s.

All 4 LED’s blinking green rapidly.

Pairing mode is active for 3 minutes. When pairing is completed, the LED will display a solid green.

Press the push-button 8 times or 4 ON cycles in 10 s to change the Wi-Fi access point mode.

All 4 LED’s blinking green rapidly.

The device is ready to connect with the new Wi-Fi access point.

Resetting

User Action

LED Indication

Status

Press the push-button 14 times or 7 ON cycles in 10 s.

All 4 LED’s blinks green.

The device is in reset mode. It is reset to the factory settings.

LED Indicator Mode

LED Indicator Mode

LED Indication

Always Off

No LED

Always On

Depending on the speed level, one of the 4 LED's become solid green that indicates the speed.

Device disconnected from the router after pairing

No LED

OTA update

No LED

Reset state / Not paired / Not added

No LED

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.