DUG_Wiser Connected Curtain Controller 2M-00

Configuring the device

Using the Wiser app, you can configure the device according to your preference.

  1. On the Home screen, tap Devices > Devices.

  2. Select the device from the list.

  3. On the Device Control Screen, tap .

    The Device Settings screen appears.

A

Device Name

Displays the device name, tap to change the device name. For more information, refer to the Renaming the device topic.

B

Change Room

Displays the assigned room of the device, tap Change Room to assign any room (such as living room, bedroom, kitchen, etc.). For more information, refer to the Changing the device location topic.

C

Device Type

Displays the device type.

D

Curtain Type

Allows you to view and modify the orientation of your curtain. You can select either Horizontal or Vertical to ensure that the curtain operates in the desired direction.

E

Device details

Allows you to set group switches, open/close duration, and configuration. When you tap Advanced Settings, you can see the following options:

  • Group Switches: Manage multiple switches as a single group.

  • Associate with other powered Z-Wave devices: Link your device with other Z-Wave devices for synchronized operation.

  • Set Open / Close Duration: Configure the duration for opening and closing actions for your device.

  • Group Association: Create associations between devices for coordinated actions.

  • View Configuration: Check the current settings and configurations of your device.

  • Set Configuration: Adjust and customize the settings of your device.

F

Calibration

Displays the product details such as manufacturer name, ID, product name, ID, and type. Also you can view the firmware version and update it if a new version is available by tapping Product Details > Firmware Version & OTA.

G

Advanced

Displays the advanced options: voltage detection & load cut-off and
Thermal cut-off.

H

Notification

Enable the Notify Me toggle button to receive device notifications.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.