DUG_Wiser Connected Curtain Controller 2M-00

Pairing the device with the Wiser Hub

Using the Wiser app, you can pair your connected curtain controller puck with the Wiser Hub to access and control the shutter.
  1. Open the Wiser app.
  2. On the Home screen, tap Devices.
    The Device Management screen appears.
  3. On the Home page, tap Devices (A).
  4. Tap + (B) to add a device.
    The Add Device page appears.
  5. Select Preferred > Curtain Controller. Enter the following Device Information and then tap Next:
    • Enter Device Name: Enter the device name.

    • Assign Existing Room: Select an existing room.

      TIP: If your room is not in the existing room list, create a new one.
    • Add New Room: Create a new room.

  6. Tap Next to pair the device with the Wiser Hub.
    • Press the pairing button 4 times in 10s.
      The LED indicator rapidly blinks green.

  7. After a few minutes, you will see the Wiser message. Tap Ok.
    You can see the newly added device on the Device Management screen under Devices.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.