0611IB1302-09

IFM Interface Registers

IFM Interface Identification

IFM Interface Firmware Revision

The IFM interface firmware revision starts at register 11776 and has a maximum length of eight registers.

The firmware revision is an ASCII string using the format XXX.YYY.ZZZ with:

  • XXX = major version (000–127)

  • YYY = minor version (000–255)

  • ZZZ = revision number (000–255)

The NULL character ends the revision number.

Address

Register

RW

Unit

Type

Range

Description

0x2DDF–0x2DEE

11744–11759

R

OCTET STRING

Device family

0x2DEF–0x2DF6

11760–11767

R

OCTET STRING

Product range

0x2DF7–0x2DFE

11768–11775

R

OCTET STRING

Product model

0x2DFF–0x2E04

11776–11781

R

OCTET STRING

Firmware revision

Serial Number for IFM Interface TRV00210 or STRV00210

The serial number of IFM interface TRV00210 or STRV00210 is composed of a maximum of 11 alphanumeric characters with the following format: PPYYWWDnnnn.

  • PP = plant code

  • YY = year of fabrication (0599)

  • WW = week of fabrication (0153)

  • D = day of fabrication (17)

  • nnnn = production number of the device on the day (00019999)

A read request of six registers is necessary to read the IFM interface serial number.

Address

Register

RW

Unit

Type

Range

Description

0x2E07

11784

R

OCTET STRING

‘PP’

0x2E08

11785

R

OCTET STRING

‘05’–‘99’

‘YY’

0x2E09

11786

R

OCTET STRING

‘01’–‘53’

‘WW’

0x2E0A

11787

R

OCTET STRING

D: ‘1’–‘7’

n: ‘0’–‘9’

‘Dn’

0x2E0B

11788

R

OCTET STRING

‘00’–‘99’

‘nn’

0x2E0C

11789

R

OCTET STRING

‘0’–‘9’

‘n’ (the NULL character ends the serial number)

Serial Number for IFM Interface LV434000

The serial number of IFM interface LV434000 is composed of a maximum of 17 alphanumeric characters with the following format: PPPPPPYYWWDLnnnn0.

  • PPPPPP = plant code (example: BATAM plant code is 0000HL)

  • YY = year of fabrication (0599)

  • WW = week of fabrication (0153)

  • D = day of fabrication (17)

  • L = line or machine number (0-9 or a-z)

  • nnnn = production number of the device on the day (00019999)

A read request of ten registers is necessary to read the IFM interface serial number.

Address

Register

RW

Unit

Type

Range

Description

0x2E5C-0x2E5E

11869-11871

R

OCTET STRING

‘PPPPPP’

0x2E5F

11872

R

OCTET STRING

‘05’–‘99’

‘YY’

0x2E60

11873

R

OCTET STRING

‘01’–‘53’

‘WW’

0x2E61

11874

R

OCTET STRING

D: ‘1’–‘7’

L: ‘0’–‘9’ or ‘a’–‘z

‘DL’

0x2E62

11875

R

OCTET STRING

‘00’–‘99’

‘nn’

0x2E63

11876

R

OCTET STRING

‘00’–‘99’

‘nn’

0x2E64-0x2E65

11877-11878

R

OCTET STRING

‘0’

‘0’ (the NULL character ends the serial number)

Current Date and Time

Address

Register

RW

Unit

Type

Range

Description

0x2E73–0x2E76

11892–11895

R-WC

DATETIME

Current date and time in DATETIME format

0x2E77–0x2E78

11896–11897

R

Seconds

INT32U

0x00–0xFFFFFFFF

Number of seconds counted since last start

Product Identification

Address

Register

RW

Unit

Type

Range

Description

0x2E7C

11901

R

INT16U

Product identification = 15146 for the IFM interface

Hardware Revision for IFM Interface LV434000

The hardware revision of IFM interface LV434000 starts at register 11922 and has a maximum length of ten registers.

The hardware revision is an ASCII string using the format XXX.YYY.ZZZ with:

  • XXX = major version (000127)

  • YYY = minor version (000255)

  • ZZZ = revision number (000255)

The NULL character ends the revision number.

Address

Register

RW

Unit

Type

Range

Description

0x2E91–0x2E96

11922–11927

R

OCTET STRING

Hardware revision

Read Device Identification

The Read Device Identification function is used to access in a standardized manner the information required to identify a device clearly. The description is made up of a set of objects (ASCII character strings).

A complete description of the Read Device Identification function is available at www.modbus.org.

The coding for the identification of the IFM interface is the following:

Name

Type

Description

Vendor name

OCTET STRING

‘Schneider Electric’ (18 characters)

Product code

OCTET STRING

'LV434000’ or 'TRV00210' (1) or ‘STRV00210’

Firmware revision

OCTET STRING

‘XXX.YYY.ZZZ’ from IFM interface revision 002.002.000

Vendor URL

OCTET STRING

‘https://www.se.com’ (33 characters)

Product name

OCTET STRING

‘ULP/Modbus-SL communication interface module’

(1) Product code returns ‘TRV00210-L’ when IFM interface TRV00210 is loaded with IFM legacy firmware. For more information, refer to MasterPacT Modbus Legacy User Guide.

@ Adrien > Confirm that 'LV434000' is returned for LV434000 with legacy firmware ??? Define the specificities of data and command for IFM legacy firmware ???

Modbus Network Parameters

Modbus Locking Pad Position

Address

Register

RW

Unit

Type

Range

Description

0x2E72

11891

R

INT16U

1–3

Modbus locking pad position

  • 1 = Modbus locking pad is on the locked position

  • 3 = Modbus locking pad is on the open position

Validity Duration of Data

Address

Register

RW

Unit

Type

Range

Description

0x306A

12395

R

s

INT16U

5–300 (in step of 5 s)

Duration of validity of data in the dataset

Auto-Speed Sensing State

Address

Register

RW

Unit

Type

Range

Description

0x306E

12399

R

INT16U

0–1

Auto-Speed sensing state

  • 0 = Auto-Speed sensing is disabled

  • 1 = Auto-Speed sensing is enabled (factory setting)

IFM Interface Modbus Address

Address

Register

RW

Unit

Type

Range

Description

0x306F

12400

R

INT16U

1–99

IFM interface Modbus address

Modbus Parity

Address

Register

RW

Unit

Type

Range

Description

0x3070

12401

R

INT16U

1–3

Modbus parity

  • 1 = no parity (none)

  • 2 = even parity (factory setting)

  • 3 = odd parity

Modbus Baud Rate

Address

Register

RW

Unit

Type

Range

Description

0x3071

12402

R

INT16U

5–8

Modbus Baud rate

  • 5 = 4800 Baud

  • 6 = 9600 Baud

  • 7 = 19200 Baud (factory setting)

  • 8 = 38400 Baud

Number of Stop Bits

Address

Register

RW

Unit

Type

Range

Description

0x3072

12403

R

INT16U

0–5

Number of stop bits

  • 0 = no change

  • 1 = standard Modbus

  • 2 = 1/2 stop bit

  • 3 = 1 stop bit

  • 4 = 1 and 1/2 stop bit

  • 5 = 2 stop bits

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?