0611IB1302-09

BSCM Module Commands

List of BSCM Module Commands and Error Codes

List of Commands

The following table lists the available BSCM module commands, their corresponding command codes and user profiles. Follow the command execution procedures accordingly Executing a Command.

Command

Command code

User profile

Open circuit breaker Open Circuit Breaker

904

Administrator or Operator

Close circuit breaker Close Circuit Breaker

905

Administrator or Operator

Reset circuit breaker Reset Circuit Breaker

906

Administrator or Operator

Enable/Inhibit close order Enable/Inhibit a Circuit Breaker Close Order

910

Administrator or Operator

Enable/disable automatic reset Enable/Disable Automatic Reset

42636

Administrator

Enable/disable reset even if SDE Enable/Disable Reset even if SDE

42637

Administrator

Preset counters Preset Counters

42638

Administrator

Set up thresholds Set Up Thresholds

42639

Administrator

Error Codes

In addition to generic error codes Result of the Command, the BSCM module commands generate the following error codes returned in register 8021:

Error Code

Description

4363 (0x110B)

BSCM module is out of order.

4503 (0x1197)

Circuit breaker is tripped. It must be reset before the command.

4504 (0x1198)

Circuit breaker is already closed.

4505 (0x1199)

Circuit breaker is already open.

4506 (0x119A)

Circuit breaker is already reset.

4507 (0x119B)

Actuator is in manual mode. Remote commands are not allowed.

4508 (0x119C)

Actuator is not present.

4510 (0x119E)

A previous command is still in progress.

4511 (0x119F)

Reset command is forbidden when SDE is set.

4512 (0x11A0)

Inhibit close order is enabled.

Any other positive error code means an internal error.

Circuit Breaker Control Commands

Open Circuit Breaker

To open the circuit breaker, set the command registers in the following way:

Address

Register

X

Unit

Type

Range

A/E

Description

0x1F3F

8000

INT16U

904

A/E

Command code = 904

0x1F40

8001

INT16U

10

A/E

Number of parameters (bytes) = 10

0x1F41

8002

INT16U

4353

A/E

Destination = 4353 (0x1101)

0x1F42

8003

INT16U

1

A/E

Security type of the command

0x1F43–

0x1F44

8004–

8005

OCTET STRING

A/E

Password of the command: Administrator or Operator user profile password

Close Circuit Breaker

To close the circuit breaker, set the command registers in the following way:

Address

Register

X

Unit

Type

Range

A/E

Description

0x1F3F

8000

INT16U

905

A/E

Command code = 905

0x1F40

8001

INT16U

10

A/E

Number of parameters (bytes) = 10

0x1F41

8002

INT16U

4353

A/E

Destination = 4353 (0x1101)

0x1F42

8003

INT16U

1

A/E

Security type of the command

0x1F43–

0x1F44

8004–

8005

OCTET STRING

A/E

Password of the command: Administrator or Operator user profile password

Reset Circuit Breaker

To reset the circuit breaker, set the command registers in the following way:

Address

Register

X

Unit

Type

Range

A/E

Description

0x1F3F

8000

INT16U

906

A/E

Command code = 906

0x1F40

8001

INT16U

10

A/E

Number of parameters (bytes) = 10

0x1F41

8002

INT16U

4353

A/E

Destination = 4353 (0x1101)

0x1F42

8003

INT16U

1

A/E

Security type of the command

0x1F43–0x1F44

8004–8005

OCTET STRING

A/E

Password of the command: Administrator or Operator user profile password

Enable/Inhibit a Circuit Breaker Close Order

To enable or inhibit a close order of the circuit breaker, set the command register in the following way:

Address

Register

X

Unit

Type

Range

A/E

Description

0x1F3F

8000

INT16U

910

A/E

Command code = 910

0x1F40

8001

INT16U

13

A/E

Number of parameters (bytes) = 13

0x1F41

8002

INT16U

4353

A/E

Destination = 4353 (0x1101)

0x1F42

8003

INT16U

1

A/E

Security type of the command

0x1F43–

0x1F44

8004–

8005

OCTET STRING

A/E

Password of the command: Administrator or Operator user profile password

0x1F45

8006

INT16U

1

A/E

  • 0 = Enable close order

  • 1 = Inhibit close order

0x1F46

8007

INT16U

A/E

Origin of the command:

256 = command sent via communication interface (IFM or IFE)

Enable/Disable Automatic Reset

The user can read the automatic reset parameters at register 564 (bit 3).

To enable/disable automatic reset, set the command registers in the following way:

Address

Register

X

Unit

Type

Range

A/E

Description

0x1F3F

8000

INT16U

42636

A/E

Command code = 42636

0x1F40

8001

INT16U

12

A/E

Number of parameters (bytes) = 12

0x1F41

8002

INT16U

4353

A/E

Destination = 4353 (0x1101)

0x1F42

8003

INT16U

1

A/E

Security type of the command

0x1F43–

0x1F44

8004–

8005

OCTET STRING

A/E

Password of the command: Administrator user profile password

0x1F45

8006

INT16U

0–1

A/E

0 = automatic reset is not enabled.

1 = automatic reset is enabled.

Enable/Disable Reset even if SDE

The user can read the reset parameters at register 564 (bit 4).

To enable/disable reset even if SDE, set the command registers in the following way:

Address

Register

X

Unit

Type

Range

A/E

Description

0x1F3F

8000

INT16U

42637

A/E

Command code = 42637

0x1F40

8001

INT16U

12

A/E

Number of parameters (bytes) = 12

0x1F41

8002

INT16U

4353

A/E

Destination = 4353 (0x1101)

0x1F42

8003

INT16U

1

A/E

Security type of the command

0x1F43–

0x1F44

8004–

8005

OCTET STRING

A/E

Password of the command: Administrator user profile password

0x1F45

8006

INT16U

0–1

A/E

0 = reset is not enabled if SDE = 1.

1 = reset is enabled even if SDE = 1.

Counter Commands

Preset Counters

The user can read the values of the counters from register 571 to 578.

To preset the counters, the user must set up the command registers the following way:

Address

Register

X

Unit

Type

Range

A/E

Description

0x1F3F

8000

INT16U

42638

A/E

Command code = 42638

0x1F40

8001

INT16U

22

A/E

Number of parameters (bytes) = 22

0x1F41

8002

INT16U

4353

A/E

Destination = 4353 (0x1100)

0x1F42

8003

INT16U

1

A/E

Security type of the command

0x1F43–

0x1F44

8004–

8005

OCTET STRING

A/E

Password of the command: Administrator user profile password

0x1F45

8006

1

INT16U

0–65535

A/E

0–65534 = preset value of the OF counter

65535 = do not preset the OF counter

0x1F46

8007

1

INT16U

0–65535

A/E

0–65534 = preset value of the SD counter

65535 = do not preset the SD counter

0x1F47

8008

1

INT16U

0–65535

A/E

0–65534 = preset value of the SDE counter

65535 = do not preset the SDE counter

0x1F48

8009

1

INT16U

0–65535

A/E

0–65534 = preset value of the open circuit breaker command counter

65535 = do not preset the open circuit breaker command counter

0x1F49

8010

1

INT16U

0–65535

A/E

0–65534 = preset value of the close circuit breaker command counter

65535 = do not preset the close circuit breaker command counter

0x1F4A

8011

1

INT16U

0–65535

A/E

0–65534 = preset value of the reset circuit breaker command counter

65535 = do not preset the reset circuit breaker command counter

Set Up Thresholds

The user can read the values of the thresholds from register 581 to 582.

To set up the thresholds, the user must set up the command registers the following way:

Address

Register

X

Unit

Type

Range

A/E

Description

0x1F3F

8000

INT16U

42639

A/E

Command code = 42639

0x1F40

8001

INT16U

22

A/E

Number of parameters (bytes) = 22

0x1F41

8002

INT16U

4353

A/E

Destination = 4353 (0x1100)

0x1F42

8003

INT16U

1

A/E

Security type of the command

0x1F43–

0x1F44

8004–

8005

OCTET STRING

A/E

Password of the command: Administrator user profile password

0x1F45

8006

1

INT16U

0–65535

A/E

0–65534 = value of the OF counter threshold

65535 = do not change the OF counter threshold

0x1F46

8007

1

INT16U

65535

A/E

65535 (no threshold is associated to the SD counter)

0x1F47

8008

1

INT16U

65535

A/E

65535 (no threshold is associated to the SDE counter)

0x1F48

8009

1

INT16U

65535

A/E

65535 (no threshold is associated to the open circuit breaker command counter)

0x1F49

8010

1

INT16U

0–65535

A/E

0–65534 = value of the close circuit breaker command counter threshold

65535 = do not change close circuit breaker command counter threshold

0x1F4A

8011

1

INT16U

65535

A/E

65535 (no threshold is associated to the reset circuit breaker command counter)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?