0611IB1302-09

IO Module Events

Event History

General Description

The event history registers describe the last 100 encountered events. The event history format corresponds to a series of 100 records. Each record is composed of 5 registers describing one event.

A read request of 5x(n) registers is necessary to read the last n event records, where 5 is the number of registers for each event record.

For example, a read request of 5x3 = 15 registers is necessary to read the last 3 event records of the event history:

  • The first five registers describe the first event record (most recent event).

  • The next five registers describe the second event record.

  • The last five registers describe the third event record.

There are two event histories, 1 per IO module.

IO Module

Address

Register

Description

IO 1

0x39A7–0x39AB

14760–14764

Event record 1 (most recent event record)

0x39AC–0x39B0

14765–14769

Event record 2

0x39A7+5x(n-1)–0x39AB+5x(n-1)

14760+5x(n-1)–14764+5x(n-1)

Event record n

0x3B96–0x3B9A

15255–15259

Event record 100

IO 2

0x455F–0x4563

17760–17764

Event record 1 (most recent event record)

0x4564–0x4568

17765–17769

Event record 2

0x455F+5x(n-1)–0x4563+5x(n-1)

17760+5x(n-1)–17764+5x(n-1)

Event record n

0x474E–0x4752

18255–18259

Event record 100

Event Record

A block request of five registers is necessary to read an event record. The order and the description of the event record registers of IO 2 are the same as those of IO 1:

Event Record 1 (Most Recent Event Record)

Register

Address

RW

Type

Description

0x39A7

14760

R

INT16U

Event code of IO 1 and IO 2

0x39A8–

0x39AA

14761–

14763

R

ULP DATE

Date and time of the event

0x39AB

14764

R

INT16U

Event type

MSB = 0 (reserved)

Event occurrence: LSB = 1

Event completion: LSB = 2

Alarm Definition

Alarms are specific events that need to be reset.

The reset mode of an alarm can be:

  • automatic: the alarm is reset automatically when the alarm is no more active.

  • manual: the alarm is reset manually with the Test/Reset push-button located on the front face of the IO module and when the alarm is no more active.

  • remote: the alarm is reset remotely with the Reset command sent via the communication and when the alarm is no more active.

Each alarm has a priority level that manages the alarm display on the FDM121 display:

  • no priority = N/A (not affected)

  • low priority = 1. No alarm display on the FDM121 display

  • medium priority = 2. The FDM121 display LED is steady ON.

  • high priority = 3. The FDM121 display LED blinks and a pop-up screen informs that the alarm has occurred.

IO Module Events and Alarms

IO 1 Events and Alarms

Code

Application

Description

Type

Priority

Reset Mode

1537 (0x0601)

General

IO1 Watchdog reset

Event

Medium

1538 (0x0602)

General

IO1 reset to factory setting

Event

Medium

1539 (0x0603)

General

IO1 failure (STOP mode)

Alarm

High

Manual or Remote

1540 (0x0604)

General

IO1 failure (ERROR mode)

Alarm

Medium

Manual or Remote

1541 (0x0605)

General

IO1 functional rotary switch position change

Event

Medium

1542 (0x0606)

General

IO1 setting locking pad rotary switch position change

Event

Medium

1543 (0x0607)

General

IO1 source address dip switch position change

Event

Medium

1552 (0x0610)

General

IO1 O1 rising edge (OFF/ON change)

Event

Low

1553 (0x0611)

General

IO1 O2 rising edge (OFF/ON change)

Event

Low

1554 (0x0612)

General

IO1 O3 rising edge (OFF/ON change)

Event

Low

1555 (0x0613)

General

IO1 I1 rising edge (OFF/ON change)

Event

Low

1556 (0x0614)

General

IO1 I2 rising edge (OFF/ON change)

Event

Low

1557 (0x0615)

General

IO1 I3 rising edge (OFF/ON change)

Event

Low

1558 (0x0616)

General

IO1 I4 rising edge (OFF/ON change)

Event

Low

1559 (0x0617)

General

IO1 I5 rising edge (OFF/ON change)

Event

Low

1560 (0x0618)

General

IO1 I6 rising edge (OFF/ON change)

Event

Low

1561 (0x0619)

General

IO1 threshold overrun on I1 counter

Alarm

Medium

Manual or Remote

1562 (0x061A)

General

IO1 threshold overrun on I2 counter

Alarm

Medium

Manual or Remote

1563 (0x061B)

General

IO1 threshold overrun on I3 counter

Alarm

Medium

Manual or Remote

1564 (0x061C)

General

IO1 threshold overrun on I4 counter

Alarm

Medium

Manual or Remote

1565 (0x061D)

General

IO1 threshold overrun on I5 counter

Alarm

Medium

Manual or Remote

1566 (0x061E)

General

IO1 threshold overrun on I6 counter

Alarm

Medium

Manual or Remote

1567 (0x061F)

General

IO1 threshold overrun on O1 counter

Alarm

Medium

Manual or Remote

1568 (0x0620)

General

IO1 threshold overrun on O2 counter

Alarm

Medium

Manual or Remote

1569 (0x0621)

General

IO1 threshold overrun on O3 counter

Alarm

Medium

Manual or Remote

1570 (0x0622)

General

IO1 I1 unforced/forced change

Event

Low

1571 (0x0623)

General

IO1 I2 unforced/forced change

Event

Low

1572 (0x0624)

General

IO1 I3 unforced/forced change

Event

Low

1573 (0x0625)

General

IO1 I4 unforced/forced change

Event

Low

1574 (0x0626)

General

IO1 I5 unforced/forced change

Event

Low

1575 (0x0627)

General

IO1 I6 unforced/forced change

Event

Low

1576 (0x0628)

General

IO1 O1 unforced/forced change

Event

Low

1577 (0x0629)

General

IO1 O2 unforced/forced change

Event

Low

1578 (0x062A)

General

IO1 O3 unforced/forced change

Event

Low

1579 (0x062B)

User-defined input acquisition

IO1 user-defined input 1

Alarm

Medium

Manual or Remote

1580 (0x062C)

User-defined input acquisition

IO1 user-defined input 2

Alarm

Medium

Manual or Remote

1581 (0x062D)

User-defined input acquisition

IO1 user-defined input 3

Alarm

Medium

Manual or Remote

1582 (0x062E)

User-defined input acquisition

IO1 user-defined input 4

Alarm

Medium

Manual or Remote

1583 (0x062F)

User-defined input acquisition

IO1 user-defined input 5

Alarm

Medium

Manual or Remote

1584 (0x0630)

User-defined input acquisition

IO1 user-defined input 6

Alarm

Medium

Manual or Remote

1585 (0x0631)

Cooling system

IO1 switchboard temperature threshold 1 overrun

Alarm

Low

Auto

1586 (0x0632)

Cooling system

IO1 switchboard temperature threshold 2 overrun

Alarm

Medium

Manual or Remote

1587 (0x0633)

Cooling system

IO1 switchboard temperature threshold 3 overrun

Alarm

High

Manual or Remote

NOTE: The alarm exit priority is fixed in IO module firmware. The value is Low, when available.

IO 2 Events and Alarms

Code

Application

Description

Type

Priority

Reset Mode

1793 (0x0701)

General

IO2 watchdog reset

Event

Medium

1794 (0x0702)

General

IO2 reset to factory settings

Event

Medium

1795 (0x0703)

General

IO2 module failure (STOP mode)

Alarm

High

Manual or Remote

1796 (0x0704)

General

IO2 module failure (ERROR mode)

Alarm

Medium

Manual or Remote

1797 (0x0705)

General

IO2 functional rotary switch position change

Event

Medium

1798 (0x0706)

General

IO2 setting locking pad rotary switch position change

Event

Medium

1799 (0x0707)

General

IO2 source address dip switch position change

Event

1808 (0x0710)

General

IO2 O1 rising edge (OFF/ON change)

Event

Low

1809 (0x0711)

General

IO2 O2 rising edge (OFF/ON change)

Event

Low

1810 (0x0712)

General

IO2 O3 rising edge (OFF/ON change)

Event

Low

1811 (0x0713)

General

IO2 I1 rising edge (OFF/ON change)

Event

Low

1812 (0x0714)

General

IO2 I2 rising edge (OFF/ON change)

Event

Low

1813 (0x0715)

General

IO2 I3 rising edge (OFF/ON change)

Event

Low

1814 (0x0716)

General

IO2 I4 rising edge (OFF/ON change)

Event

Low

1815 (0x0717)

General

IO2 I5 rising edge (OFF/ON change)

Event

Low

1816 (0x0718)

General

IO2 I6 rising edge (OFF/ON change)

Event

Low

1817 (0x0719)

General

IO2 threshold overrun on I1 counter

Alarm

Medium

Manual or Remote

1818 (0x071A)

General

IO2 threshold overrun on I2 counter

Alarm

Medium

Manual or Remote

1819 (0x071B)

General

IO2 threshold overrun on I3 counter

Alarm

Medium

Manual or Remote

1820 (0x071C)

General

IO2 threshold overrun on I4 counter

Alarm

Medium

Manual or Remote

1821 (0x071D)

General

IO2 threshold overrun on I5 counter

Alarm

Medium

Manual or Remote

1822 (0x071E)

General

IO2 threshold overrun on I6 counter

Alarm

Medium

Manual or Remote

1823 (0x071F)

General

IO2 threshold overrun on O1 counter

Alarm

Medium

Manual or Remote

1824 (0x0720)

General

IO2 threshold overrun on O2 counter

Alarm

Medium

Manual or Remote

1825 (0x0721)

General

IO2 threshold overrun on O3 counter

Alarm

Medium

Manual or Remote

1826 (0x0722)

General

IO2 I1 unforced/forced change

Event

Low

1827 (0x0723)

General

IO2 I2 unforced/forced change

Event

Low

1828 (0x0724)

General

IO2 I3 unforced/forced change

Event

Low

1829 (0x0725)

General

IO2 I4 unforced/forced change

Event

Low

1830 (0x0726)

General

IO2 I5 unforced/forced change

Event

Low

1831 (0x0727)

General

IO2 I6 unforced/forced change

Event

Low

1832 (0x0728)

General

IO2 O1 unforced/forced change

Event

Low

1833 (0x0729)

General

IO2 O2 unforced/forced change

Event

Low

1834 (0x072A)

General

IO2 O3 unforced/forced change

Event

Low

1835 (0x072B)

User-defined input acquisition

IO2 user-defined input 1

Alarm

Medium

Manual or Remote

1836 (0x072C)

User-defined input acquisition

IO2 user-defined input 2

Alarm

Medium

Manual or Remote

1837 (0x072D)

User-defined input acquisition

IO2 user-defined input 3

Alarm

Medium

Manual or Remote

1838 (0x072E)

User-defined input acquisition

IO2 user-defined input 4

Alarm

Medium

Manual or Remote

1839 (0x072F)

User-defined input acquisition

IO2 user-defined input 5

Alarm

Medium

Manual or Remote

1840 (0x0730

User-defined input acquisition

IO2 user-defined input 6

Alarm

Medium

Manual or Remote

1841 (0x0731)

Cooling system

IO2 switchboard temperature threshold 1 overrun

Alarm

Low

Auto

1842 (0x0732)

Cooling system

IO2 switchboard temperature threshold 2 overrun

Alarm

Medium

Manual or Remote

1843 (0x0733)

Cooling system

IO2 switchboard temperature threshold 3 overrun

Alarm

High

Manual or Remote

NOTE: The alarm exit priority is fixed in IO firmware. The value is Low, when available.

IO 1 and IO 2 Events and Alarms

Code

Application

Description

Type

Priority

Reset Mode

2304 (0x0900)

Cradle management

Cradle position discrepancy

Alarm

Medium

Manual or Remote

2305 (0x0901)

Cradle management

Cradle connected contact change

Alarm

Low

Manual or Remote

2306 (0x0902)

Cradle management

Cradle disconnected contact change

Alarm

Low

Manual or Remote

2307 (0x0903)

Cradle management

Cradle test contact change

Alarm

Low

Manual or Remote

2308 (0x0904)

Cradle management

Remove device from cradle and put it back

Alarm

Medium

Manual or Remote

2309 (0x0905)

Cradle management

Cradle has reached its maximum number of operations

Alarm

High

Manual or Remote

2310 (0x0906)

Cradle management

Remaining service life of cradle is below alarm threshold

Alarm

Medium

Manual or Remote

2311 (0x0907)

Cradle management

New MicroLogic control unit has been detected.

Alarm

High

Manual or Remote

2432 (0x0980

Drawer management

Drawer position discrepancy

Alarm

Medium

Manual or Remote

2560 (0x0A00)

Load control

Auxiliary contact of the load contactor 1 is not closed

Alarm

Medium

Manual or Remote

2561 (0x0A01)

Load control

Auxiliary contact of the load contactor 1 is not opened

Alarm

Medium

Manual or Remote

2816 (0x0B00)

Predefined input acquisition

Earth leakage trip signal contact (SDV)

Alarm

Medium

Manual or Remote

2817 (0x0B01)

Predefined input acquisition

Control voltage presence contact

Alarm

Medium

Manual or Remote

2818 (0x0B02)

Predefined input acquisition

Surge protection status contact

Alarm

Medium

Manual or Remote

2819 (0x0B03)

Predefined input acquisition

Surge failure contact

Alarm

Medium

Manual or Remote

2820 (0x0B04)

Predefined input acquisition

Switch-disconnector ON/OFF indication contact (OF)

Alarm

Medium

Manual or Remote

2821 (0x0B05)

Predefined input acquisition

Fuse blown indication contact

Alarm

Medium

Manual or Remote

2822 (0x0B06)

Predefined input acquisition

Emergency stop

Alarm

High

Manual or Remote

2823 (0x0B07)

Cooling system

Switchboard temperature contact

Alarm

Medium

Manual or Remote

2824 (0x0B08)

Cooling system

Switchboard ventilation contact

Alarm

Medium

Manual or Remote

2825 (0x0B09)

Cooling system

Switchboard door contact

Alarm

Medium

Manual or Remote

3072 (0x0C00)

Protection settings

Discrepancy with ERMS OFF order and ERMS ON order (MasterPacT NT/NW and PowerPacT P- and R-frame only)

Alarm

High

Manual or Remote

3328 (0x0D00)

General

Critical hardware modules discrepancy

Alarm

High

Auto

3329 (0x0D01)

General

Critical firmware modules discrepancy

Alarm

High

Auto

3330 (0x0D02)

General

Non-critical hardware modules discrepancy

Alarm

Medium

Auto

3331 (0x0D03)

General

Non-critical firmware modules discrepancy

Alarm

Medium

Auto

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?