0611IB1302-09

MicroLogic Trip Unit Commands

List of MicroLogic Trip Unit Commands and Error Codes

List of Commands

The following table lists the available MicroLogic trip unit commands, their corresponding command codes and user profiles. Follow the command execution procedures accordingly Executing a Command.

Command

Command code

User profile

Long-time protection Long-Time Protection

45192

Administrator

Short-time protection Short-Time Protection

45193

Administrator

Instantaneous protection Instantaneous Protection

45194

Administrator

Ground-fault protection Ground-Fault Protection

45195

Administrator

Neutral protection Neutral Protection

45197

Administrator

Jam protection Jam Protection

45448

Administrator

Underload protection Underload Protection

45449

Administrator

Unbalance protection Unbalance Protection

45450

Administrator

Long-start protection Long-Start Protection

45451

Administrator

Acknowledge a latched output Acknowledge a Latched Output

46216

Administrator or Operator

Acknowledge a trip Acknowledge a Trip

46217

Administrator

Set up ENVT presence Set Up ENVT Presence

46472

Administrator

Reset minimum/maximum Reset Minimum/Maximum

46728

Administrator or Operator

Start/stop synchronization Start/Stop Synchronization

46729

Administrator or Operator

Power flow sign configuration Power Flow Sign Configuration

47240

Administrator

Power factor sign configuration Power Factor Sign Configuration

47241

Administrator

Energy accumulation mode configuration Energy Accumulation Mode Configuration

47242

Administrator

Current demand configuration Current Demand Configuration

47243

Administrator

Power demand configuration Power Demand Configuration

47244

Administrator

Set up nominal voltage Vn display Set Up Nominal Voltage Vn Display

47245

Administrator

Error Codes

Error codes generated by MicroLogic trip units are the generic error codes Result of the Command.

MicroLogic Trip Unit Protection Commands

Long-Time Protection

The user can read the long-time protection parameters from register 8754 to 8763 Long-Time Protection Parameters.

To set the long-time protection parameters, the user must set up the command registers the following way:

Address

Register

X

Unit

Type

Range

A/E

Description

0x1F3F

8000

INT16U

45192

A/E

Command code = 45192

0x1F40

8001

INT16U

18

A/E

Number of parameters (bytes) = 18

0x1F41

8002

INT16U

5121

A/E

Destination = 5121 (0x1401)

0x1F42

8003

INT16U

1

A/E

Security type of the command

0x1F43–

0x1F44

8004–

8005

OCTETSTRING

A/E

Password of the command: Administrator user profile password

0x1F45

8006

1

A

INT16U

A/E

Ir pick-up value. The Ir range depends on the nominal current In and on the position of the MicroLogic trip unit rotary switch 1 (Ir).

0x1F46

8007

1

ms

INT16U

500–

16000

A/E

tr time delay (distribution application only)

tr = 500, 1000, 2000, 4000, 8000, 16000 ms

0x1F47

8008

INT16U

5–30

A/E

Motor class (motor application only)

Possible values = 5, 10, 20, 30 s

0x1F48

8009

INT16U

1–2

A/E

Cool fan (motor application only)

1 = auto, 2 = motor

Short-Time Protection

The user can read the short-time protection parameters from register 8764 to 8773 Short-Time Protection Parameters.

To set the short-time protection parameters, the user must set up the command registers the following way:

Address

Register

X

Unit

Type

Range

A/E

Description

0x1F3F

8000

INT16U

45193

A/E

Command code = 45193

0x1F40

8001

INT16U

16

A/E

Number of parameters (bytes) = 16

0x1F41

8002

INT16U

5121

A/E

Destination = 5121 (0x1401)

0x1F42

8003

INT16U

1

A/E

Security type of the command

0x1F43–

0x1F44

8004–

8005

OCTETSTRING

A/E

Password of the command: Administrator user profile password

0x1F45

8006

10

INT16U

(1)

A/E

Isd coefficient, adjustable in step of 5.

Isd pick-up value = (Ir) x (Isd coefficient) / 10

0x1F46

8007

1

ms

INT16U

0–400

A/E

tsd time delay

tsd= 0, 100, 200, 300, 400 ms

If tsd = 0 ms, then I2t must be Off.

0x1F47

8008

INT16U

0–1

A/E

Type of protection: 0 = I2t On, 1 = I2t Off

For motor application, tsd = 0 ms and I2t is Off (fixed values).

(1) For distribution application, the range is 15–100. For motor application, the range is 50–130.

Instantaneous Protection

The user can read the instantaneous protection parameters from register 8774 to 8783 Instantaneous Protection Parameters.

To set the instantaneous protection parameters, the user must set up the command registers the following way:

Address

Register

X

Unit

Type

Range

A/E

Description

0x1F3F

8000

INT16U

45194

A/E

Command code = 45194

0x1F40

8001

INT16U

12

A/E

Number of parameters (bytes) = 12

0x1F41

8002

INT16U

5121

A/E

Destination = 5121 (0x1401)

0x1F42

8003

INT16U

1

A/E

Security type of the command

0x1F43–

0x1F44

8004–

8005

OCTET STRING

A/E

Password of the command: Administrator user profile password

0x1F45

8006

10

INT16U

(1)

A/E

Ii coefficient, adjustable in step of 5.

Ii pick-up value = (In) x (Ii coefficient) / 10

(1) The Ii coefficient range depends on the circuit breaker size:

  • for 100–160 A, the range is 15–150.

  • for 250–400 A, the range is 15–120.

  • for 630 A, the range is 15–110.

Ground-Fault Protection

The user can read the ground-fault protection parameters from register 8784 to 8793 Ground-Fault Protection Parameters.

To set the ground-fault protection parameters, the user must set up the command registers the following way:

Address

Register

X

Unit

Type

Range

A/E

Description

0x1F3F

8000

INT16U

45195

A/E

Command code = 45195

0x1F40

8001

INT16U

16

A/E

Number of parameters (bytes) = 16

0x1F41

8002

INT16U

5121

A/E

Destination = 5121 (0x1401)

0x1F42

8003

INT16U

1

A/E

Security type of the command

0x1F43–

0x1F44

8004–

8005

OCTET STRING

A/E

Password of the command: Administrator user profile password

0x1F45

8006

100

INT16U

(1)

A/E

Ig coefficient, adjustable in step of 5. The value is defined by the position of the MicroLogic trip unit rotary switch 2 (Ig).

Ig pick-up value = (In) x (Ig coefficient) / 100

0x1F46

8007

1

ms

INT16U

0–400

A/E

tg time delay

tg = 0, 100, 200, 300, 400 ms

If tg = 0 ms, then I2t must be Off.

0x1F47

8008

INT16U

0–1

A/E

Type of protection: 0 = I2t On, 1 = I2t Off

For motor application, tg = 0 ms and I2t is Off (fixed values).

(1) The Ig coefficient depends on the sensor rating In and the MicroLogic trip unit rotary switch if it exists.

For example, 0 (protection Off) or 0.40 In to In in step of 0.05. The Ig coefficient cannot be set using the command interface when the MicroLogic rotary switch position Ig is Off.

Neutral Protection

The neutral protection is only available when system type in register 3314 is 30 or 41 System Type.

The user can read the neutral protection parameters from register 8916 to 8919 Neutral Protection Parameters.

To set the neutral protection registers, the user must set up the command registers the following way:

Address

Register

X

Unit

Type

Range

A/E

Description

0x1F3F

8000

INT16U

45197

A/E

Command code = 45197

0x1F40

8001

INT16U

12

A/E

Number of parameters (bytes) = 12

0x1F41

8002

INT16U

5121

A/E

Destination = 5121 (0x1401)

0x1F42

8003

INT16U

1

A/E

Security type of the command

0x1F43–

0x1F44

8004–

8005

OCTET STRING

A/E

Password of the command: Administrator user profile password

0x1F45

8006

INT16U

0–3

A/E

Neutral coefficient pickup value

0 = Off

1 = 0.5

2 = 1.0

3 = OSN

Jam Protection

The jam protection is available for motor application only.

The user can read the jam protection parameters from registers 8900 to 8903 Jam Protection Parameters.

To set the jam protection parameters, the user must set up the command registers the following way:

Address

Register

X

Unit

Type

Range

A/E

Description

0x1F3F

8000

INT16U

45448

E

Command code = 45448

0x1F40

8001

INT16U

16

E

Number of parameters (bytes) = 16

0x1F41

8002

INT16U

5121

E

Destination = 5121 (0x1401)

0x1F42

8003

INT16U

1

E

Security type of the command

0x1F43–

0x1F44

8004–

8005

OCTET STRING

E

Password of the command: Administrator user profile password

0x1F45

8006

INT16U

0–1

E

Activation: 0 = Off, 1 = On

0x1F46

8007

10

INT16U

10–80

E

Ijam coefficient, adjustable in step of 1.

Ijam pick-up value = (Ir) x (Ijam coefficient) / 10

0x1F47

8008

1

s

INT16U

1–30

E

tjam time delay

Underload Protection

The underload protection is available for motor application only.

The user can read the underload protection parameters from register 8908 to 8911 Underload Protection Parameters.

To set the underload protection parameters, the user must set up the command registers the following way:

Address

Register

X

Unit

Type

Range

A/E

Description

0x1F3F

8000

INT16U

45449

E

Command code = 45449

0x1F40

8001

INT16U

16

E

Number of parameters (bytes) = 16

0x1F41

8002

INT16U

5121

E

Destination = 5121 (0x1401)

0x1F42

8003

INT16U

1

E

Security type of the command

0x1F43–

0x1F44

8004–

8005

OCTET STRING

E

Password of the command: Administrator user profile password

0x1F45

8006

INT16U

0–1

E

Activation: 0 = Off, 1 = On

0x1F46

8007

100

INT16U

30–90

E

Iunderload coefficient, adjustable in step of 1.

Iunderload pick-up value = (Ir) x (Iunderload) / 100

0x1F47

8008

1

s

INT16U

1–200

E

tunderload time delay

Unbalance Protection

The unbalance protection is available for motor application only.

The user can read the unbalance protection parameters from register 8904 to 8907 Unbalance Protection Parameters.

To set the unbalance protection parameters, the user must set up the command registers the following way:

Address

Register

X

Unit

Type

Range

A/E

Description

0x1F3F

8000

INT16U

45450

E

Command code = 45450

0x1F40

8001

INT16U

14

E

Number of parameters (bytes) = 14

0x1F41

8002

INT16U

5121

E

Destination = 5121 (0x1401)

0x1F42

8003

INT16U

1

E

Security type of the command

0x1F43–

0x1F44

8004–

8005

OCTET STRING

E

Password of the command: Administrator user profile password

0x1F45

8006

1

%

INT16U

10–40

E

Iunbal coefficient

0x1F46

8007

1

s

INT16U

1–10

E

tunbal time delay

Long-Start Protection

The long-start protection is available for motor application only.

The user can read the underload protection parameters from register 8912 to 8915 Long-Start Protection Parameters.

To set the long-start protection parameters, the user must set up the command registers the following way:

Address

Register

X

Unit

Type

Range

A/E

Description

0x1F3F

8000

INT16U

45451

E

Command code = 45451

0x1F40

8001

INT16U

16

E

Number of parameters (bytes) = 16

0x1F41

8002

INT16U

5121

E

Destination = 5121 (0x1401)

0x1F42

8003

INT16U

1

E

Security type of the command

0x1F43–

0x1F44

8004–

8005

OCTET STRING

E

Password of the command: Administrator user profile password

0x1F45

8006

INT16U

0–1

E

Activation: 0 = Off, 1 = On

0x1F46

8007

10

INT16U

10–80

E

Ilongstart coefficient, adjustable in step of 1.

Ilongstart pick-up value = (Ir) x (Ilongstart coefficient) / 10

0x1F47

8008

1

s

INT16U

1–200

E

tlongstart time delay

Event Commands

Acknowledge a Latched Output

The user can read the SDx module outputs parameters from register 9801 to 9810 Configuration of the SDx Module.

To acknowledge a latched output, the user must set up the command registers the following way:

Address

Register

X

Unit

Type

Range

A/E

Description

0x1F3F

8000

INT16U

46216

A/E

Command code = 46216

0x1F40

8001

INT16U

12

A/E

Number of parameters (bytes) = 12

0x1F41

8002

INT16U

5121

A/E

Destination = 5121 (0x1401)

0x1F42

8003

INT16U

1

A/E

Security type of the command

0x1F43–

0x1F44

8004–

8005

OCTET STRING

A/E

Password of the command: Administrator or Operator user profile password

0x1F45

8006

INT16U

1–2

A/E

1 = relay 1, 2 = relay 2

Acknowledge a Trip

To acknowledge a trip, the user must set up the command registers the following way:

Address

Register

X

Unit

Type

Range

A/E

Description

0x1F3F

8000

INT16U

46217

A/E

Command code = 46217

0x1F40

8001

INT16U

10

A/E

Number of parameters (bytes) = 10

0x1F41

8002

INT16U

5121

A/E

Destination = 5121 (0x1401)

0x1F42

8003

INT16U

1

A/E

Security type of the command

0x1F43–

0x1F44

8004–

8005

OCTET STRING

A/E

Password of the command: Administrator user profile password

Measurement Configuration Commands

Set Up ENVT Presence

The user can read the ENVT (External Neutral Voltage Tap) presence parameters at register 3314 System Type.

To set up ENVT presence, the user must set up the command registers the following way:

Address

Register

X

Unit

Type

Range

A/E

Description

0x1F3F

8000

INT16U

46472

E

Command code = 46472

0x1F40

8001

INT16U

12

E

Number of parameters (bytes) = 12

0x1F41

8002

INT16U

5121

E

Destination = 5121 (0x1401)

0x1F42

8003

INT16U

1

E

Security type of the command

0x1F43–

0x1F44

8004–

8005

OCTET STRING

E

Password of the command: Administrator user profile password

0x1F45

8006

INT16U

0–1

E

0 = ENVT is not present.

1 = ENVT is present.

Reset Minimum/Maximum

The reset minimum/maximum command resets the minimum values of real-time measurements (registers 1300 to 1599) and the maximum values of real-time measurements (registers 1600 to 1899) Minimum/Maximum Values of Real-Time Measurements.

The reset minimum/maximum command resets the energy measurements (registers 2000 to 2025) Energy Measurements.

The reset minimum/maximum command resets the peak demand measurements (registers 2200 to 2237) Demand Measurements.

The user can read the minimum and maximum values of current, voltage, and frequency measurements and the corresponding dates from register 29780 to 29827 Minimum/Maximum VAB Voltage Measurements.

The user can read the dates of the reset minimum/maximum command from register 2900 to 2929 Minimum/Maximum Measurements Reset Time.

To reset minimum/maximum values of measurements, the user must set up the command registers the following way:

Address

Register

Type

Range

A/E

Bit

Description

0x1F3F

8000

INT16U

46728

Command code = 46728

0x1F40

8001

INT16U

12

Number of parameters (bytes) = 12

0x1F41

8002

INT16U

5121

Destination = 5121 (0x1401)

0x1F42

8003

INT16U

1

Security type of the command

0x1F43–

0x1F44

8004–

8005

OCTET STRING

Password of the command: Administrator or Operator user profile password

0x1F45

8006

INT16U

Reset minimum/maximum of metering variables:

  • To reset the metering variable, set the bit to 1.

  • To keep the current values, set the bit to 0.

A/E

0

Reset minimum/maximum current (IA, IB, IC, IN, Imax, Ig, IΔn, Iavg, and Iunbal)

E

1

Reset minimum/maximum voltage (VAB, VAC, VBC, VAN, VBN, VCN, VavgL-L, VavgL-N, and Vunbal)

E

2

Reset minimum/maximum power (active power, reactive power, apparent power, and distortion power)

E

3

Reset minimum/maximum power factor and cosϕ

E

4

Reset minimum/maximum total harmonic distortion (THD)

E

5

Reset peak of current demand

E

6

Reset peak of active power, reactive power, and apparent power demand

E

7

Reset minimum/maximum frequency

E

8

Reset minimum/maximum thermal image (motor application only)

E

9

Reset energy (active, reactive, apparent)

10–15

Reserved

Start/Stop Synchronization

The start/stop synchronization command is used to start or stop the calculation of the current or power demand. The first command starts the calculation, the next command updates the value of current or power demand, and then restarts the calculation. The time period between 2 commands must be less than 1 hour.

To start/stop synchronization, the user must set up the command registers the following way:

Address

Register

X

Unit

Type

Range

A/E

Description

0x1F3F

8000

INT16U

46729

E

Command code = 46729

0x1F40

8001

INT16U

12

E

Number of parameters (bytes) = 12

0x1F41

8002

INT16U

5121

E

Destination = 5121 (0x1401)

0x1F42

8003

INT16U

1

E

Security type of the command

0x1F43–

0x1F44

8004–

8005

OCTET STRING

E

Password of the command: Administrator or Operator user profile password

0x1F45

8006

INT16U

E

Start/stop synchronization = 1

Power Flow Sign Configuration

The user can read the power flow sign configuration at register 3316 Power Flow Sign.

To set the power flow sign parameters, the user must set up the command registers the following way:

Address

Register

X

Unit

Type

Range

A/E

Description

0x1F3F

8000

INT16U

47240

E

Command code = 47240

0x1F40

8001

INT16U

12

E

Number of parameters (bytes) = 12

0x1F41

8002

INT16U

5121

E

Destination = 5121 (0x1401)

0x1F42

8003

INT16U

1

E

Security type of the command

0x1F43–

0x1F44

8004–

8005

OCTET STRING

E

Password of the command: Administrator user profile password

0x1F45

8006

INT16U

0–1

E

Power flow sign:

0 = the active power flows from upstream (top) to downstream (bottom) (factory setting).

1 = the active power flows from downstream (bottom) to upstream (top).

NOTE: The setting of the power flow sign can reset the content of the energy measurement registers excluding the cumulative energy measurements.

Power Factor Sign Configuration

The user can read the power factor sign configuration at register 3318 Power Factor Sign.

To set the power factor sign parameters, the user must set up the command registers the following way:

Address

Register

X

Unit

Type

Range

A/E

Description

0x1F3F

8000

INT16U

47241

E

Command code = 47241

0x1F40

8001

INT16U

12

E

Number of parameters (bytes) = 12

0x1F41

8002

INT16U

5121

E

Destination = 5121 (0x1401)

0x1F42

8003

INT16U

1

E

Security type of the command

0x1F43–

0x1F44

8004–

8005

OCTET STRING

E

Password of the command: Administrator user profile password

0x1F45

8006

INT16U

0–2

E

Sign convention for the power factor and the fundamental power factor (cosϕ):

0 = IEC convention

2 = IEEE convention (factory setting)

Energy Accumulation Mode Configuration

The user can read the energy accumulation mode configuration at register 3324 Energy Accumulation Mode.

To set the energy accumulation mode parameters, the user must set up the command registers the following way:

Address

Register

X

Unit

Type

Range

A/E

Description

0x1F3F

8000

INT16U

47242

E

Command code = 47242

0x1F40

8001

INT16U

12

E

Number of parameters (bytes) = 12

0x1F41

8002

INT16U

5121

E

Destination = 5121 (0x1401)

0x1F42

8003

INT16U

1

E

Security type of the command

0x1F43–

0x1F44

8004–

8005

OCTET STRING

E

Password of the command: Administrator user profile password

0x1F45

8006

INT16U

0–1

E

Energy accumulation mode:

0 = absolute accumulation (factory setting)

1 = signed accumulation

Current Demand Configuration

The user can read the duration of the current demand calculation window at register 3352 Demand Time.

The user can read the current demand parameters from register 2200 to 2207 Current Demand.

To start current demand, the user must set up the command registers the following way:

Address

Register

X

Unit

Type

Range

A/E

Description

0x1F3F

8000

INT16U

47243

E

Command code = 47243

0x1F40

8001

INT16U

12

E

Number of parameters (bytes) = 12

0x1F41

8002

INT16U

5121

E

Destination = 5121 (0x1401)

0x1F42

8003

INT16U

1

E

Security type of the command

0x1F43–

0x1F44

8004–

8005

OCTET STRING

E

Password of the command: Administrator user profile password

0x1F45

8006

Min

INT16U

5–60

E

Duration of the current demand calculation window, adjustable in step of 1.

The factory setting is 15 minutes (sliding).

Power Demand Configuration

The user can read the power demand calculation method from register 3354 to 3355 Demand Time.

The user can read the power demand parameters from register 2224 to 2237 Active Power Demand.

To start power demand, the user must set up the command registers the following way:

Address

Register

X

Unit

Type

Range

A/E

Description

0x1F3F

8000

INT16U

47244

E

Command code = 47244

0x1F40

8001

INT16U

14

E

Number of parameters (bytes) = 14

0x1F41

8002

INT16U

5121

E

Destination = 5121 (0x1401)

0x1F42

8003

INT16U

1

E

Security type of the command

0x1F43–

0x1F44

8004–

8005

OCTET STRING

E

Password of the command: Administrator user profile password

0x1F45

8006

Min

INT16U

0–5

E

Power demand calculation method (window type):

0 = sliding

2 = fixed

5 = synchronized to communication

The factory setting is 0 (sliding).

0x1F46

8007

Min

INT16U

5–60

E

Duration of the power demand calculation window, adjustable in step of 1.

The factory setting is 15 minutes.

Set Up Nominal Voltage Vn Display

The user can read the nominal voltage at register 9616 Nominal Voltage.

To set the nominal voltage Vn display parameters, the user must set up the command registers the following way:

Address

Register

X

Unit

Type

Range

A/E

Description

0x1F3F

8000

INT16U

47245

E

Command code = 47245

0x1F40

8001

INT16U

12

E

Number of parameters (bytes) = 12

0x1F41

8002

INT16U

5121

E

Destination = 5121 (0x1401)

0x1F42

8003

INT16U

1

E

Security type of the command

0x1F43–

0x1F44

8004–

8005

OCTET STRING

E

Password of the command: Administrator user profile password

0x1F45

8006

V

INT16U

0–65535

E

Nominal voltage Vn (factory setting = 400 V)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?