AMI Configuration Batch Scripts

Execute the Configure_AMI.bat located in the path C:\Program Files (x86)\Miner and Miner\Responder\Integration\Configuration\Ami

This script must be executed on all machines where RxIF Server has been installed.

This script requires the following files:

  • AmiArchiveQueriesConfig.xupdate

  • AmiDatabaseSchemaConfig.xupdate

  • AMISubmitRulesConfig.xupdate

  • Ping_Request_DatabaseSchemaConfig.xupdate

  • PingMeterControlStylesConfig.xupdate

TIP: If the installation is an upgrade or patch fix, please save a backup copy of SubmitRulesConfig.xml, DatabaseSchemaConfig.xml, ControlStylesConfig.xml and Miner.Responder.DataServices.exe.config.xml from the C:\Program Files (x86)\Miner and Miner\Responder\Server folder. After the batch script use an XML file compare function to compare the new configurations with the backup configurations and verify changes (Notepad++ or XMLPad).

The files changed by the xupdates are as follows:

  • ArchiveSchemaConfig

    • Adds the Ami Restore Time column to RX_CALLS_ARCHIVE table.

  • DatabaseSchemaConfig

    • Adds the Ami Restore Time column to RX_CALLS and RX_CALLS_HISTORY tables.

    • Adds the Ping Requests and Meters tables.

    • Adds the PingRequest_Meters relationship.

    • Adds Tilt to the AMI_EVENT domain.

    • Adds the RXINT_PING_STATUS and RXINT_CONFIG domains.

  • SubmitRulesConfig

    • Adds the UpdateIncidentRelatedHistoryTables submit rule if it doesn’t already exist.

  • ControlStylesConfig

    • Adds RxIntDevicePingMeterRequest to the following ControlStyles:

      • IncidentGrid

      • IncidentGridAllRegions

      • DevicesGrid

      • DevicesGridAllRegions,

      • EditIncident_DeviceGrid

      • SelectedIncident_DeviceGrid

      • EditIncident_CustomerGrid

      • SelectedIncident_CustomerGrid

    • Adds the RxIntPingGrid control style.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?