Ping Downstream from Device

IMPORTANT: This optional configuration is only for AMI users.

Enable the Ping Downstream Meters tool in Responder Explorer (for a device) and in ArcMap (for snap to a device) using these steps.

  1. Add the RXINTPINGDOWNSTREAMMETERS model name to the Responder Object Class domain.
  2. Assign RXINTPINGDOWNSTREAMMETERS model name to Transformer, Fuse, and other necessary network device feature classes.
  3. Restart Responder Services.
  4. Make sure your configuration is correct in Responder Explorer by right-clicking on any transformer to see if Ping Downstream Meters is available in the right-click menu. In ArcMap you can check the configuration by executing the Ping Downstream Meter tool.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?