Server

To install RxIF Server:
  1. Run the RxIF.Server_####_Release.msi installer. In the Welcome dialog, click Next.
    TIP: The #### in the installer name represents the release number. For example, if you are installing 10.6.1b, the installer name is RxIF.Server_1061b_Release.msi, and the 10.8.1 installer name is RxIF.Server_1081_Release.msi.
  2. If ArcFM is already installed, the same install location will be used. Otherwise, ensure the location is set to C:\Program Files (x86)\Miner and Miner\ or use the Browse button to select it, then click Next.
  3. To start the installation, click Install.

The installation is complete and the files are deployed to C:\Program Files (x86)\Miner and Miner\Responder\Server, or wherever Responder Server is installed.

The configuration files required by AMI and IVR will be installed to C:\Program Files (x86)\Miner and Miner\Responder\Integration\Configuration.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?