CIM - Common Interface Module (optional module)

  1. Run the RxIF.CimService_####_Release.msi installer. In the Welcome dialog, click Next.
    TIP: The #### in the installer name represents the release number. For example, if you are installing 10.6.1b, the installer name is RxIF.CimService_1061b_Release.msi, and the 10.8.1 installer name is RxIF.CimService_1081_Release.msi.
  2. Ensure that the location is set to the IIS web root - IE C:\inetpub\wwwroot\ - or use the Browse button to select the location.
  3. Choose your database and click Next.
  4. Enter the credentials for the database and click Next.
  5. If Responder Web is installed, the same install location will be used. Otherwise ensure that the location is set to the IIS web root, e.g., C:\inetpub\wwwroot\, or use the Browse button to select it, and click Next.
  6. Start the installation by clicking Install.
  7. The installation will complete and the files will be deployed to Miner.Responder.RxIF.CimServices in the web root, e.g.C:\inetpub\wwwroot\Miner.Responder.RxIF.CimServices.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?