Add the Export to CAD Workflow to Portal

  1. Open the VertiGIS Studio Workflow Designer application and log in to the Portal where you want to save the Export to Cad workflow.
  2. Click File > Import.
  3. Navigate to the location of the Export to CAD workflow file: e.g., SupplementalFiles\ExportToCAD\Workflow\ExportToCAD.json.
  4. Select it and click Open.
  5. You don’t need to make any changes to the workflow. Just click File > Save As.
  6. Edit the name if desired and click Save.
  7. The Export to CAD workflow is now available on your Portal.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?