Managing Security with Tokens

To allow communication with ArcGIS Server or Portal, a token must be supplied as an argument to the Export to CAD Workflow in ArcFM Web.
  1. Go to https://yourGISServer.domain.com/arcgis/admin/generateToken and enter the appropriate information for your environment. To minimize token expiration frequency, the life span can be adjusted via Server Admin > Home > security > tokens. For example, an expiration value of 525600 equates to 365 days.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?