Connectors
Coaxial connectors are the interconnection devices found at each end of a coaxial cable assembly.
Connectors Properties
Manufacturer
The manufacturer of the component.
Model Number (required)
The component's model number. The model number is required to be unique across all resources of the same type.
Company ID
The ID your company assigns to the component. It is recommended that you use unique company IDs. You will see a warning if you type a company ID that is not unique, but you are allowed to continue with a non-unique ID.
Description
A short description of the component.
GIS Symbology
GIS Symbology provides you with the ability to specify symbology text for various component specifications in Catalog. This text is published to GIS with DHFC features and can be used as a basis for symbology.
Catalog Id
The GUID assigned to the component.
Is Deprecated (default: not selected)
Toggle to mark the component as deprecated.
Connectors Type
From the drop-down, select Housing to Housing or Pin.
Forward Loss and Return Loss
- 
                  
Remove: Click the Remove button to the right of the value that you want to delete.
 - 
                  
Add: Type the appropriate value(s) and click the Add button to the right of the value(s) you are adding.
 - 
                  
Edit an existing value: Double-click the existing value and type a new value, then click Update to save all changes.
- 
                        
Forward Loss: The amount of forward signal loss at particular frequencies.
 - 
                        
Return Loss: The amount of return signal loss for at particular frequencies.
 
 -