Power Inserters
Power inserters are passive devices used to add AC power to the center conductor of a coaxial cable for the purpose of powering active devices.
Power Inserters Details
Manufacturer
The manufacturer of the component.
Model Number (required)
The component's model number. The model number is required to be unique across all resources of the same type.
Company ID
The ID your company assigns to the component. It is recommended that you use unique company IDs. You will see a warning if you type a company ID that is not unique, but you are allowed to continue with a non-unique ID.
Description
A short description of the component.
GIS Symbology
GIS Symbology provides you with the ability to specify symbology text for various component specifications in Catalog. This text is published to GIS with DHFC features and can be used as a basis for symbology.
Catalog Id
The GUID assigned to the component.
Is Deprecated (default: not selected)
Toggle to mark the component as deprecated.
Power Inserters Properties
Point Size (required): Assign a point value to a component based on physical size. With a consistent point value system you will be able to determine how much equipment can fit inside an enclosure. For example, if you have a pedestal rated to hold 30 points worth of components, then you can situate three 2-port taps rated at 10 points each into the box. A fourth 2-port tap would total 40 points, exceeding the rated 30 points of the pedestal.
Output Port Count (required)
The maximum number of output ports.
Power Inserter Loss
- 
                        
Remove: Click the Remove button to the right of the value that you want to delete.
 - 
                        
Add: Type the appropriate value(s) and click the Add button to the right of the value(s) you are adding.
 - 
                        
Edit an existing value: Double-click the existing value and type a new value, then click Update to save all changes.
- 
                                 
Forward Loss (required): The amount of forward signal loss at particular frequencies.
 - 
                                 
Return Loss (required): The amount of return signal loss at particular frequencies.
 
 -