RFNode_RFNodeCoaxPort
There are two versions of this relationship:
- 
                  
RFNode_RFNodeCoaxPort for the as-built representation.
 - 
                  
RFNode_RFNodeCoaxPort_D for the in-design representation.
 
For step-by-step instructions, read the topic RFCoupler_RFCouplerPort. Because the steps are the same, only the relevant properties are included in this topic.
RFNode_RFNodeCoaxPort, the As-Built Relationship
| 
                         Relationship Class Property  | 
                     
                         Value or Choice  | 
                  
|---|---|
| 
                         Name  | 
                     
                         RFNode_RFNodeCoaxPort  | 
                  
| 
                         Origin Table or Feature Class  | 
                     
                         RFNode  | 
                  
| 
                         Destination Table or Feature Class  | 
                     
                         RFNodeCoaxPort  | 
                  
| 
                         Relationship Type  | 
                     
                         Simple  | 
                  
| 
                         Forward Label  | 
                     
                         RFNodeCoaxPort 
 IMPORTANT: The Forward Label you
                              type while creating the relationship must match the EsriBuiltName
                              entry in the Schema.xml file for this component. 
                        
                      | 
                  
| 
                         Backward Label  | 
                     
                         RFNode  | 
                  
| 
                         Message Direction  | 
                     
                         None (no messages propagated)  | 
                  
| 
                         Cardinality  | 
                     
                         1–M (one to many)  | 
                  
| 
                         Relationship Attributes  | 
                     
                         No, I do not want to add attributes to this relationship class  | 
                  
| 
                         Primary Key  | 
                     
                         NetworkId  | 
                  
| 
                         Foreign Key  | 
                     
                         NodeId  | 
                  
RFNode_RFNodeCoaxPort_D, the In-Design Relationship
| 
                         Relationship Class Property  | 
                     
                         Value or Choice  | 
                  
|---|---|
| 
                         Name  | 
                     
                         RFNode_RFNodeCoaxPort_D  | 
                  
| 
                         Origin Table or Feature Class  | 
                     
                         RFNode_D  | 
                  
| 
                         Destination Table or Feature Class  | 
                     
                         RFNodeCoaxPort_D  | 
                  
| 
                         Relationship Type  | 
                     
                         Simple  | 
                  
| 
                         Forward Label  | 
                     
                         SECom.ARCFM.RFNodeCoaxPort 
 IMPORTANT: The Forward
                              Label you type while creating the relationship must match the EsriDesignName
                              entry in the Schema.xml file for this component. 
                        
                      | 
                  
| 
                         Backward Label  | 
                     
                         SECom.ARCFM.RFNode  | 
                  
| 
                         Message Direction  | 
                     
                         None (no messages propagated)  | 
                  
| 
                         Cardinality  | 
                     
                         1–M (one to many)  | 
                  
| 
                         Relationship Attributes  | 
                     
                         No, I do not want to add attributes to this relationship class  | 
                  
| 
                         Primary Key  | 
                     
                         NetworkId  | 
                  
| 
                         Foreign Key  | 
                     
                         NodeId  |