Enumerated Data Types
DHFC uses specific enumerations for some of the attribute fields. These enumerated data types are defined by the application and inform certain functionality. For that reason, they can only use the values declared, and they cannot be edited at your company site. However, you are able to map the same enumerated data type values to a domain defined by your GIS.
|
IMPORTANT: Do not change the
coded domain values in your GIS once they have been put into production
or have designs associated with them. If you change the coded values
post-implementation, you inherently orphan data and the application
fails to load.
|
Required
|
Feature Class/Object Table |
Field Name |
Enumeration |
Description |
|---|---|---|---|
|
RFCoupler and RFCoupler_D |
CouplerType |
0 |
TwoWay |
|
1 |
ThreeWay |
||
|
2 |
DirectionalCoupler |
||
|
3 |
ThreeWayUnbalanced |
||
|
Any that have the Workflow_Status field |
Workflow_Status |
0 |
AsBuilt |
|
1 |
Proposed |
||
|
UndergroundJunction and UndergroundJunction_D |
UndergroundJunctionType |
0 |
SharpTurn |
|
1 |
BoreHole |
Optional
|
Feature Class/Object Table |
Field Name |
Enumeration |
Description |
|---|---|---|---|
|
Any with an OH/UG Demarcation |
RFOverheadUnderground |
0 |
OH |
|
1 |
UG |
||
|
RFNode/RFNode_D |
SegmentationMode |
0 |
Non Segmented |
|
2 |
Two Way |
||
|
3 |
Three Way |
||
|
4 |
Four Way |
||
|
RFSplice/RFSplice_D |
SpliceType |
0 |
PBA |
|
1 |
Straight |
||
|
2 |
Block |
||
|
3 |
Demarcation |
||
|
RFTap/RFTap_D |
ConditioningPluginType |
20 |
CE |
|
21 |
CS |
||
|
22 |
RA |
||
|
23 |
HT |