UndergroundSpan_Duct
Because there is no in-design representation of UndergroundSpan or Duct, there is only one version of this relationship:
-
UndergroundSpan_Duct for the as-built representation.
For step-by-step instructions, read the topic RFCoupler_RFCouplerPort. Because the steps are the same, only the relevant properties are included in this topic.
UndergroundSpan_Duct, the As-Built Relationship
|
Relationship Class Property |
Value or Choice |
|---|---|
|
Name |
UndergroundSpan_Duct |
|
Origin Table or Feature Class |
UndergroundSpan |
|
Destination Table or Feature Class |
Duct |
|
Relationship Type |
Simple |
|
Forward Label |
Duct
IMPORTANT: The Forward Label you type while
creating the relationship must match the EsriBuiltName entry in the
Schema.xml file for this component.
|
|
Backward Label |
UndergroundSpan |
|
Message Direction |
None (no messages propagated) |
|
Cardinality |
1–M (one to many) |
|
Relationship Attributes |
No, I do not want to add attributes to this relationship class |
|
Primary Key |
NetworkId |
|
Foreign Key |
UndergroundSpanId |