Structures Dataset
The following tables display the required feature classes and fields that compose the Structures Dataset.
AddressPoint
<Table CoaxName="AddressPointData" EsriDesignName="AddressPoint" EsriBuiltName="AddressPoint">
This is a point feature class with the following required fields:
|
Field Name |
Data Type |
Notes |
|---|---|---|
|
NetworkID |
GUID |
Unique identifier for the component or record. |
|
ObjectID |
Object ID |
Esri Object Id for the feature or object. |
|
AerialStructureId |
GUID |
NetworkId of the overhead structure that this component is associated with; an empty GUID means this component is not associated with any overhead structure. |
|
CommercialMDUCount |
Long Integer |
The number of commercial service locations inside a Multi-Dwelling Unit (MDU) |
|
HouseNo |
String |
The house number of the address point. |
|
ResidentialMDUCount |
Long Integer |
The number of residential service locations inside a Multi-Dwelling Unit (MDU) |
|
StreetName |
String |
The street name for the address point. This field is required for DHFC. |
|
SymbolRotation |
Double |
The component’s symbol rotation. |
|
TapId |
GUID |
The NetworkId of the as-built tap that feeds the address point. |
|
TapId_D |
GUID |
The NetworkId of the proposed tap that feeds the address point. |
|
UGStructureId |
GUID |
The NetworkId of the underground structure that this component is associated with; an empty GUID means this component is not associated with any underground structure. |
MduBoundary
<Table CoaxName="MduBoundaryData" EsriDesignName="MduBoundary" EsriBuiltName="MduBoundary">
This is a polygon feature class with the following required fields:
|
Field Name |
Data Type |
Notes |
|---|---|---|
|
NetworkID |
GUID |
Unique identifier for the component or record. |
|
ObjectID |
Object ID |
Esri Object Id for the feature or object. |
|
Name |
String |
Name of boundary |
MduPathElement
<Table CoaxName="MduPathElementData" EsriDesignName="MduPathElement" EsriBuiltName="MduPathElement">
This is a line feature class with the following required fields:
MduPolygonElement
<Table CoaxName="MduPolygonElementData" EsriDesignName="MduPolygonElement" EsriBuiltName="MduPolygonElement">
This is a polygon feature class with the following required fields:
|
Field Name |
Data Type |
Notes |
|---|---|---|
|
NetworkID |
GUID |
Unique identifier for the component or record. |
|
ObjectID |
Object ID |
Esri Object Id for the feature or object. |
|
MduBoundaryID |
GUID |
The NetworkId of the Multi-Dwelling Unit (MDU) the polygon element is associated with |
|
Style |
String |
A .json representation of the style of the MDU element |
MduTextElement
<Table CoaxName="MduTextElementData" EsriDesignName="MduTextElement" EsriBuiltName="MduTextElement">
This is a point feature class with the following required fields:
|
Field Name |
Data Type |
Notes |
|---|---|---|
|
NetworkID |
GUID |
Unique identifier for the component or record. |
|
ObjectID |
Object ID |
Esri Object Id for the feature or object. |
|
MduBoundaryId |
GUID |
The NetworkId of the Multi-Dwelling Unit (MDU) the text element is associated with |
|
Style |
String |
A .json representation of the style of the MDU element |
|
Text |
String |
The text to be displayed |
OverheadSpan
<Table CoaxName="OverheadSpanData" EsriDesignName="OverheadSpan" EsriBuiltName="OverheadSpan">
This is a line feature class with the following required fields:
|
Field Name |
Data Type |
Notes |
|---|---|---|
|
NetworkID |
GUID |
Unique identifier for the component or record. |
|
ObjectID |
Object ID |
Esri Object Id for the feature or object. |
|
IsInMDU |
Short Integer |
Boolean (typically Yes/No) indicating whether or not the component is found within an Multi-Dwelling Unit (MDU). |
|
Length |
Double |
The length of the span; this value is automatically provided by DHFC based on the strand length, but it can be overridden by the user |
RFDrop
<Table CoaxName="RFDropData" EsriDesignName="RFDrop" EsriBuiltName="RFDrop">
This is a line feature class with the following required fields:
|
Field Name |
Data Type |
Notes |
|---|---|---|
|
NetworkID |
GUID |
Unique identifier for the component or record. |
|
ObjectID |
Object ID |
Esri Object Id for the feature or object. |
|
Workflow_Status |
String |
WorkflowState enumeration: AsBuilt and Proposed; for more information, refer to the topic Enumerated Data Types. |
SupportStructure
<Table CoaxName="SupportStructureData" EsriDesignName="SupportStructure" EsriBuiltName="SupportStructure">
This is a point feature class with the following required fields:
|
Field Name |
Data Type |
Notes |
|---|---|---|
|
NetworkID |
GUID |
Unique identifier for the component or record. |
|
ObjectID |
Object ID |
Esri Object Id for the feature or object. |
|
CommercialCount |
Integer |
The number of commercial service locations associated with the structure |
|
IsInMDU |
Short Integer |
Boolean (typically Yes/No) indicating whether or not the component is found within an Multi-Dwelling Unit (MDU). |
|
PoleType |
Short Integer |
The application requires the following four values: CableOnly, PowerAndPhone, MidSpan, and Demarcation. Beyond that, other values may be added to the coded value domain and mapped to the GIS domain. See the topic Schema.xml Configuration File for more information. |
|
ResidentialCount |
Long Integer |
The number of residential service locations associated with the structure |
|
RiserDistance |
Double |
The height of a riser, if one is present |
|
SymbolRotation |
Double |
The component’s symbol rotation. |
UndergroundJunction
<Table CoaxName="RFUndergroundJunctionData" EsriDesignName="RFUndergroundJunction" EsriBuiltName="RFUndergroundJunction">
This is a point feature class with the following required fields:
|
Field Name |
Data Type |
Notes |
|---|---|---|
|
NetworkID |
GUID |
Unique identifier for the component or record. |
|
ObjectID |
Object ID |
Esri Object Id for the feature or object. |
|
IsInMDU |
Short Integer |
Boolean (typically Yes/No) indicating whether or not the component is found within an Multi-Dwelling Unit (MDU). |
|
SymbolRotation |
Double |
The component’s symbol rotation. |
|
Type |
Short Integer |
UndergroundJunctionType enumeration: SharpTurn, BoreHole; for more information, see the topic Enumerated Data Types |
UndergroundSpan
<Table CoaxName="UndergroundSpanData" EsriDesignName="UndergroundSpan" EsriBuiltName="UndergroundSpan">
This is a line feature class with the following required fields:
|
Field Name |
Data Type |
Notes |
|---|---|---|
|
NetworkID |
GUID |
Unique identifier for the component or record. |
|
ObjectID |
Object ID |
Esri Object Id for the feature or object. |
|
IsInMDU |
Short Integer |
Boolean (typically Yes/No) indicating whether or not the component is found within an Multi-Dwelling Unit (MDU). |
|
Length |
Double |
The length of the underground span |
UndergroundStructure
<Table CoaxName="UndergroundStructureData" EsriDesignName="UndergroundStructure" EsriBuiltName="UndergroundStructure">
This is a point feature class with the following required fields:
|
Field Name |
Data Type |
Notes |
|---|---|---|
|
NetworkID |
GUID |
Unique identifier for the component or record. |
|
ObjectID |
Object ID |
Esri Object Id for the feature or object. |
|
CommercialCount |
Short Integer |
The number of commercial service locations associated with the structure |
|
IsInMDU |
Short Integer |
Boolean (typically Yes/No) indicating whether or not the component is found within an Multi-Dwelling Unit (MDU). |
|
ResidentialCount |
Long Integer |
The number of residential service locations associated with the structure |
|
StructureType |
String |
The type of underground structure the component represents; DHFC handles the types Demarcation and AptBox with specific functionality, and all other structure types are treated as the same generic structure; all structure type values should correspond to a defined Underground Structure Type from a DHFC catalog spec |
|
SymbolRotation |
Double |
The component’s symbol rotation. |