RFNode_RFSegmentableNodeBoundary
There are two versions of this relationship:
- 
                  
RFNode_RFSegmentableNodeBoundary for the as-built representation.
 - 
                  
RFNode_RFSegmentableNodeBoundary_D for the in-design representation.
 
For step-by-step instructions, read the topic RFCoupler_RFCouplerPort. Because the steps are the same, only the relevant properties are included in this topic.
RFNode_RFSegmentableNodeBoundary, the As-Built Relationship
| 
                         Relationship Class Property  | 
                     
                         Value or Choice  | 
                  
|---|---|
| 
                         Name  | 
                     
                         RFNode_RFSegmentableNodeBoundary  | 
                  
| 
                         Origin Table or Feature Class  | 
                     
                         RFNode  | 
                  
| 
                         Destination Table or Feature Class  | 
                     
                         RFSegmentableNodeBoundary  | 
                  
| 
                         Relationship Type  | 
                     
                         Simple  | 
                  
| 
                         Forward Label  | 
                     
                         RFSegmentableNodeBoundary  | 
                  
| 
                         Backward Label  | 
                     
                         RFNode  | 
                  
| 
                         Message Direction  | 
                     
                         None (no messages propagated)  | 
                  
| 
                         Cardinality  | 
                     
                         1–M (one to many)  | 
                  
| 
                         Relationship Attributes  | 
                     
                         Yes, I would like to add attributes to this relationship class  | 
                  
| 
                         Field Name: NetworkId  | 
                  |
| 
                         Data Type: Text  | 
                  |
| 
                         Allow NULL Values: Yes  | 
                  |
| 
                         Length: 150  | 
                  |
| 
                         Origin Primary Key  | 
                     
                         NetworkId  | 
                  
| 
                         Origin Foreign Key  | 
                     
                         NodeNetworkId  | 
                  
| 
                         Destination Primary Key  | 
                     
                         NetworkId  | 
                  
| 
                         Destination Foreign Key  | 
                     
                         SegmentableBoundaryNetworkId  | 
                  
RFNode_RFSegmentableNodeBoundary_D, the In-Design Relationship
| 
                         Relationship Class Property  | 
                     
                         Value or Choice  | 
                  
|---|---|
| 
                         Name  | 
                     
                         RFNode_RFSegmentableNodeBoundary_D  | 
                  
| 
                         Origin Table or Feature Class  | 
                     
                         RFNode_D  | 
                  
| 
                         Destination Table or Feature Class  | 
                     
                         RFSegmentableNodeBoundary_D  | 
                  
| 
                         Relationship Type  | 
                     
                         Simple  | 
                  
| 
                         Forward Label  | 
                     
                         RFSegmentableNodeBoundary_D  | 
                  
| 
                         Backward Label  | 
                     
                         RFNode_D  | 
                  
| 
                         Message Direction  | 
                     
                         None (no messages propagated)  | 
                  
| 
                         Cardinality  | 
                     
                         1–M (one to many)  | 
                  
| 
                         Relationship Attributes  | 
                     
                         Yes, I would like to add attributes to this relationship class  | 
                  
| 
                         Field Name: NetworkId  | 
                  |
| 
                         Data Type: Text  | 
                  |
| 
                         Allow NULL Values: Yes  | 
                  |
| 
                         Length: 150  | 
                  |
| 
                         Origin Primary Key  | 
                     
                         NetworkId  | 
                  
| 
                         Origin Foreign Key  | 
                     
                         NodeNetworkId  | 
                  
| 
                         Destination Primary Key  | 
                     
                         NetworkId  | 
                  
| 
                         Destination Foreign Key  | 
                     
                         SegmentableBoundaryNetworkId  |