Voltage Regulator

Because voltage is different at any point on a feeder, voltage regulators provide voltage control where feeders of different lengths and diverse load conditions are supplied from the same substation bus. Feeder voltage regulators can be single or three-phase and operate from 25 to 400 kVA. The 32-step design regulates line load from 10 percent above (boost) to 10 percent below (buck) normal line voltage. Operating over a 20 percent range, voltage change per step is 5/8 percent.

Voltage regulators vary the AC supply or source voltage to the customer to maintain the voltage within desired limits. Voltage provided by regulators is changed using a tap-changing switch to adjust the number of secondary windings. Bypass switches allow a regulator to be removed for normal service without interrupting the downstream load.

The DESIGNBANK model name is used by the Work Function tool in Designer. It designates a banked feature in the network.

VoltageRegulator inherits attributes from the abstract classes ElectricDevice and TransformerBank. Any model names assigned to these classes should be assigned to VoltageRegulator as well.

Associations: None

Subtypes: Single Phase Overhead, Two Phase Overhead, Three Phase Overhead, Three Phase Pad-Mounted. The use of subtypes is optional. The Subtype attribute can be removed if subtypes aren't used in the model.

Model Names: DESIGNBANK

Attributes:

Field Name

Field Type

Description

BoostPercent

text

Code indicating tap setting for increase in capacity achieved by raising the maximum voltage level; domain values include 4 percent, 6 percent, etc.

BuckPercent

text

Code indicating tap setting for increase in capacity achieved by lowering the minimum voltage level; domain values include 4 percent, 6 percent, etc.

BypassSwitch

text

Code indicating presence of BypassSwitch used to de-energize voltage regulator; domain values are Yes or No.

HighSideConfiguration

text

Configuration of primary side of Transformer; domain values include SinglePhaseLine-Ground, Open, SinglePhaseLine-Line, Wye. HIGHSIDECONFIGURATION

RatedkVA[A,B,C]

double

Sum of rated kVA of related transformer units, per phase; domain values include 100kVA, 1000kVA, etc. The RatedKVA on Transformer validation rule uses the RATEDKVA model name on this field. Designer's Secondary Circuit Analysis also uses this model name.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.