Motor Starting Calculation

his calculation determines voltage flicker or the amount voltage fluctuates briefly when a motor (such as an air conditioner) is started.

The magnitude of the inrush kVA for a motor is computed as the product of the motor's horsepower and a multiplier derived from its NEMA code rating. The resulting inrush current IINRUSH is computed as

  

where Vo is the nominal secondary circuit voltage

The voltage flicker VFLICKER due to motor starting at bus i is then computed as

 

  VFLICKER = | IINRUSH | ZXFR + ZPATH |

 

where ZXFR is the transformer impedance and ZPATH is the total impedance of the conductor path joining bus i to the transformer secondary bus.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.