DUG_AC Fan controller_CLP-00

Creating a schedule

The fan controller can be controlled and triggered by a schedule. Once the schedule is set, your system will follow the active schedule. You can create or modify the schedules at any time.
  1. On the Home page, tap All devices > Iconic Fan Controller.
  2. Tap Schedule > Add schedule to add a schedule.
  3. Set the time (A).
  4. Tap Repeat (B) to select the days you want to set the schedule.
  5. Tap Note (C), enter the note and tap Confirm.
  6. Tap the toggle switch (D) to turn On the Notification for the schedule. The app will send a notification that the scheduled task is executed at the time of schedule.
  7. Tap Fan Speed (E) and select the required speed:
    • Low
    • Medium
    • High
  8. Tap Save.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.