DUG_AC Fan controller_CLP-00

Device Orientation

The Fan Controller can be installed in 4 different orientations. This feature allows the user/installer to select the orientation of the low/medium/high speed LEDs to maintain the same sequence across different fan controllers.

On the Settings page, tap Device Orientation and select any of the following:

Horizontal Left

Horizontal Right

Vertical Top

Vertical Bottom

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.