DUG_AC Fan controller_CLP-00

LED indication

Pairing the device

User Action

LED Indication

Status

Press and hold the push button for > 8 s times.

For Zigbee, LED blinks amber.

For Bluetooth, LED blinks red green.

Pairing mode is active for 30 seconds. When pairing is completed, LED glows green for a few seconds before turning Off.

Changing protocol

User Action

LED Indication

Status

Short press the push-button 3 times and long press once for > 20 s.

LED blinks red rapidly indicating commence of protocol change.

On successful change in protocol:

  • Zigbee to Bluetooth - No colour indication, white back light only.

  • Bluetooth to Zigbee - Flashing Amber LED (Indicating that device is in pairing mode), if pairing is not completed will become solid Amber

Resetting the device

User Action

LED Indication

Status

Short press the push button 3 times and hold it down once for > 10 s.

LED blinks red once per second.

For Zigbee, the device is reset to the factory settings after 10 seconds. The device then restarts and the LED blinks amber indicating that it is ready for pairing.

For Bluetooth, .the device is reset to the factory settings after 10 seconds and the device turns off.

LED indicator mode

LED indicator mode

Speed

LEDs

Timeout

Locator*

Always On

Low

LED1

0

No

Medum

LED1 and LED2

High

LED1, LED2, and LED3

Off

LED1, LED2, LED3, and LED4

Act as a Locator

Low

LED1

5 s

Yes

Medum

LED1 and LED2

High

LED1, LED2, and LED3

Off

LED1, LED2, LED3, and LED4

On with Timeout

Low

LED1

5 s

No

Medum

LED1 and LED2

High

LED1, LED2, and LED3

Off

LED1, LED2, LED3, and LED4

*Glows all four LEDs in lesser brightness after the time out

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.