DUG_AC Fan controller_CLP-00

Manual operation

You can turn on/off or control the fan speed manually.

Shortly press the push button to turn on the fan at low speed, then press it again to change the speed to medium and then again to high.

Press and hold the push-button for 1 s to turn off the fan.
You can also turn off the fan by short pressing the push button once when it is at high speed

TIP: You can change LED behavior in Wiser app setting:

For Zigbee, refer Zigbee LED indication setting.

For Bluetooth, refer Bluetooth LED indication setting.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.