DUG_AC Fan controller_CLP-00

Operating the device using app

Using the Wiser app, you can turn on/off and regulate the fan speed.

  1. On Home page, select the fan controller and tap power button (A) to turn on/off the fan.

  2. Once fan is turned on, select the required speed (B).

NOTE: During timer mode, the fan controller automatically turns off after a specified period of time. Refer Using timer mode.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?