DUG_AC Fan controller_CLP-00

Pairing Zigbee device manually

You can pair the device to Wiser system manually with or without installed code.
  1. On the Home page, tap +.
  2. Tap Iconic A.C. fan controller ZB and select the required Wiser Hub on the slide-up menu.
  3. Select any one of the options to add device (A):
    • Add Device with Install Code
    • Add Device without Install Code
    TIP: It is highly recommended to add the device with Install code.
  4. To pair the device with install code, tap Add Device with Install Code to display the slide-up menu. Select any one of the options (B):
    • Scan Install Code: you can scan the device for the install code.
      TIP: The QR code is located on the push button.
    • Enter Install Code Manually: you can manually enter the install code from the device.
      TIP: The install code is located on the device's top.
    After scanning or entering the install code, proceed to Step 6.

  5. To pair the device without install code, tap Add Device without Install Code.
  6. Press and hold the push-button for > 8 s to enter pairing mode.
  7. In the app, tap Confirm the indicator blinking rapidly and then tap Start Configuration (C).
    Wait for a few seconds until the LED turns green.
  8. Once the device is added in the app, tap Done.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?