DUG_AC Fan controller_CLP-00

Removing the device from Wiser system

Using the Wiser app, you can remove the fan controller from the device list.
  1. On the Home page, tap All devices and select the Iconic Fan Controller which must to be removed.
  2. Tap to display more details.
  3. Tap Remove and Factory Reset Device (A) and tap Confirm.
    TIP: On the Home page, tap and hold the Iconic Fan Controller to remove the device.
    NOTE: By removing the device, you will reset the device and all related data is erased. If you have a problem with the reset, then refer to resetting the device.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?