990-6287B-001

Transfer a Single UPS from Normal Mode to Static Bypass Mode

  1. From the home screen on the display select Control > Inverter ON/OFF > Turn Single INV OFF.

    The UPS transfers from normal to static bypass mode without an interruption to the load.

    The LEDs on the user interface show as follows:

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.