990-6287B-001

Configure the Output Settings

NOTICE
risk of equipment damage
Only trained personnel following the required training must make modifications to the UPS system parameters.
Failure to follow these instructions can result in equipment damage.
  1. From the home screen of the display select Settings > Advanced settings > Output settings.
  2. Set the Output frequency (Hz). Choose between 50 and 60 Hz.
  3. Set the Output voltage (V). Choose between 380, 400, and 415 V.
  4. Set the output voltage compensation (%). Choose a value between –5 and 5.
  5. Tap Save settings.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.