990-91189F-001

Communication Interfaces

NOTE: Route the signal cables separately from the power cables.

10-15 kVA 400 V UPS

  1. Dry contacts

  2. Parallel ports

  3. USB (for service)

  4. RS485

  5. RS232 (for service)

  6. Network management card (NMC)

  7. Cold start (optional)

20 kVA 400 V / 10 kVA 208 V UPS

  1. Dry contacts

  2. Parallel ports

  3. USB (for service)

  4. RS485

  5. RS232 (for service)

  6. Network management card (NMC)

  7. Cold start (optional)

30 kVA 400 V / 15-20 kVA 208 V UPS

  1. Dry contacts

  2. Parallel ports

  3. USB (for service)

  4. RS485

  5. RS232 (for service)

  6. Network management card (NMC)

  7. Cold start (optional)

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.