990-91189F-001

Appendix: Switch/Breaker Details

3:1 UPS

  Model Switch/Breaker Description Switch or Breaker
10 kVA

UIB

OSMC65H4C32

32A 4P

Breaker

SIB

OSMC65H4C32

32A 4P

Breaker

UOB

A9S68263 

63A 2P

Switch

MBB

A9S68163

63A 1P

Switch

BB

A9S68332

32A 3P

Switch (for UPSs with internal batteries)

15 kVA

UIB

OSMC65H4C40

40A 4P

Breaker

 

SIB

OSMC65H4C40

40A 4P

Breaker

 

UOB

A9S68280

80A 2P

Switch

 

MBB

A9S68180 

80A 1P

Switch

 

BB

A9S68363 

63A 3P

Switch (for UPSs with internal batteries)

20 kVA

UIB

OSMC65H4C63

63A 4P

Breaker

 

SIB

OSMC65H4C63

63A 4P

Breaker

 

UOB

A9S68292

125A 2P

Switch

 

MBB

A9S68192

125A 1P

Switch

 

BB

A9S68363

63A 3P

Switch (for UPSs with internal batteries)

30 kVA

UIB

A9S68480

500VAC 80A 4P

Switch

 

SIB

A9S68491

100A 4P

Switch

 

UOB

A9S68491

100A 4P

Switch

 

MBB

A9S68280

80A 2P

Switch

 

BB

A9S68391

100A 3P

Switch (for UPSs with internal batteries)

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.