990-91189F-001

Remove the UPS from the Pallet

  1. Move the UPS to the final installation area using a forklift.
  2. Remove the shipping materials and the ramp from the UPS.
  3. Place the ramp on the pallet and fasten with the provided bolts.
  4. Loosen the bolts and remove the shipping brackets. Dispose of the shipping brackets.
  5. Roll the UPS down from the pallet.
  6. Move the UPS to its final location and use a wrench to lower the levelling feet. Ensure that the cabinet is level.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.