990-91189F-001

Input Contacts and Output Relays

Input Contacts

NOTE: J2 is reserved for the internal battery temperature sensor which is installed from factory.

Input connections are considered 24 VDC Class 2/SELV.

Input Contacts for UPSs with Batteries

Output Relays

Output relay connection: Maximum 3A/240 VAC.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.