990-91189F-001

Connect the Power Cables in the 30 kVA UPS

  1. Ensure that all breakers are in the OFF (open) position.
  2. Remove the lower plate.

    Rear View of the 30 kVA UPS

  3. In dual mains systems, remove the single mains bracket.

    Rear View of the 30 kVA UPS

  4. Route the power cables through the bottom of the UPS.
  5. Connect the PE cable to the PE busbar.

    Rear View of the 30 kVA UPS

  6. Connect the input cables, output cables, and bypass cables (if applicable).
  7. Connect the battery cables if the UPS should have external batteries for extended runtime.
    NOTE: Ensure that the type and number of blocks are the same as the internal batteries.
  8. Reinstall the lower plate.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.