DUG_ELKO - Wiser Room Thermostat_WH-00

Resetting the device

The Room Thermostat can be reset manually at any time, e.g., if the Hub is replaced. To remove the device from a heating system and join another system.
To reset the Room Thermostat:
  1. Remove the batteries and re-insert them.
  2. When the “Wiser” startup screen appears, press the + and - buttons at the same time for 20 seconds until the unit restarts.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.