DUG_ELKO - Wiser Room Thermostat_WH-00

Troubleshooting

Symptom

Possible cause

Solution

The Room Thermostat screen goes blank.

Batteries may be low or drained

Replace the batteries.

Unable to set the room temperature

Wiser Hub signal is weak or not connected to the WIFI network.

Check for a Wi-Fi® signal.

Unable to set the room temperature, control are disabled.

Check room details if only if Room thermostat is alone in the room and the hub is not connected to the boiler relay.

Add a heating device to this room will enable to control temperature.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.