DUG_ELKO - Wiser Room Thermostat_WH-00

Identifying the device

Using the Wiser Home app, you can identify a Room Thermostat from the other available devices in the room.
To identify the Room Thermostat:
  1. On the Home screen, tap .
  2. Tap Devices > Room Thermostat > Identify (A).
    NOTE:
    • This feature displays an exclamation mark on the Room Thermostat screen, so you can identify the actual device. It may take up to a minute to display an exclamation mark on the Room Thermostat screen.

    • The Room Thermostat displays an exclamation mark until you tap OK.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.