DUG_ELKO - Wiser Room Thermostat_WH-00

Replacing the batteries

Replace the batteries when the battery level is low. The battery level can be seen in the Room Thermostat display top-right corner. It can also be viewed in the Wiser Home app under Settings > Devices.
Follow the steps below to replace the batteries:
  1. Open the battery compartments.
  2. Replace the batteries.
    TIP: Make sure that the polarity of the batteries (+ and -) are in the right direction. The polarity is indicated on the terminals of the device.
    NOTICE
    Use only standard, non-rechargeable AA Alkaline batteries
    • Do not use rechargeable batteries, Zinc Carbon, or Zinc Chloride batteries.
    • Rechargeable batteries are not optimized for Wiser device systems.
    Failure to follow these instructions can result in equipment damage.
  3. Close the battery compartments.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.