ESXP2G001EN-Trans-05

General Methodology for Designing Digital Applications for Large Buildings and Critical Facilities

Building a digital electrical installation is much easier if you follow the steps below:

Understand the desired outcomes of the end user.

 

Do you need help?

Find an EcoXpert Partner

See EcoXpert

 

Define the electrical installation, depending on the building’s type and constraints.

See:

 
 

Define the system design considerations for your installation.

See Defining the System Design Considerations

 
 

Select the required digital applications and learn how to implement them in the installation.

See Overview of Digital Applications

Select the correct:

 

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?