ESXP2G001EN-Trans-05

Purpose of this Document

Target Audience

This design guide is intended for certified EcoXpert partners, System Integrators, Specifiers, electrical distribution designers, and other qualified personnel who are responsible for the design of projects.

Objective

The objective of EcoStruxure Power is to offer a range of digital applications to fulfill customers’ needs in large buildings and critical facilities such as data centers, large hotels, healthcare, industrial facilities, etc.

This document details the system design considerations for the electrical installation that must be taken into account when designing a digital architecture.

Also, it explains how to select the most appropriate digital applications according to the end users' needs, and how to implement these applications to meet the system design considerations.

This technical guide provides a special focus on all the necessary building blocks required at each level, for each application.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?