ESXP2G001EN-Trans-05

Structure of the Guide

Part Defining the System Design Considerations addresses design considerations of the electrical installation in the context of system communications, data recording and timestamping, time synchronization, data processing, data quality management, and cybersecurity.

Part Selecting and Implementing the Digital Applications outlines the values provided by all EcoStruxure Power applications and provides information on how to select the most appropriate applications according to the end user's needs. It also explains how to implement these applications in a defined electrical architecture to be compliant with the system design considerations. It identifies all necessary building blocks required at each level, for each application, and how to connect those building blocks to Edge Control software and/or to cloud-based Analytics and Services.

The Appendix provides a brief description of all key connected products, Edge Control software, and cloud-based Services.

The Bibliography provides links to useful documentation.

Information about our EcoXpert and Green Premium programs is available at the end of the guide.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?