ESXP2G001EN-Trans-05

Data Recording Options

In the EcoStruxure Power digital platform, data recording can occur at various levels of the architecture. Connected products, depending on their level of sophistication, can record data as follows:

  • All data recorded and timestamped on board

  • Only event and alarm data recorded and timestamped on board

  • No onboard logging; real-time data only. Data recording and timestamping are performed by a data logger or Edge Control software.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?